Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.Target |
Post.Target.AXIS_SYMMETRY3D |
static Post.Target |
Post.Target.CUTTING_PLANE |
static Post.Target |
Post.Target.FREE_FACEES |
static Post.Target |
Post.Target.VOLUME |
Modifier and Type | Method and Description |
---|---|
static Post.Target |
Post.Target.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Target |
Post.Target.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Target[] |
Post.Target.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetTarget(int postviewId,
Post.Target target)
Set the target operator in the input postview id.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.