Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.Legend |
Post.Legend.COLORBAR_ONLY |
static Post.Legend |
Post.Legend.DETAILED |
static Post.Legend |
Post.Legend.HEADER_ONLY |
Modifier and Type | Method and Description |
---|---|
static Post.Legend |
Post.Legend.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Legend |
Post.Legend.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Legend[] |
Post.Legend.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetLegend(int postviewId,
boolean showLegend,
Post.Legend legend)
Deprecated.
Deprecated in NX8.5.0. Use
Post.postviewSetShowHeader(int, nxopen.cae.Post.ShowHeader) and Post.postviewSetColorbar(int, nxopen.cae.Post.Colorbar) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.