Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.GroupVisibility |
Post.GroupVisibility.HIDE |
static Post.GroupVisibility |
Post.GroupVisibility.SHOW |
static Post.GroupVisibility |
Post.GroupVisibility.SHOW_ONLY |
Modifier and Type | Method and Description |
---|---|
static Post.GroupVisibility |
Post.GroupVisibility.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.GroupVisibility |
Post.GroupVisibility.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.GroupVisibility[] |
Post.GroupVisibility.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewApplyUserGroupVisibility(int postviewId,
int[] usergroupIds,
Post.GroupVisibility visibility)
Control visibility of one or more usergroups with immediate effect.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.