Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static NodesBetweenNodesBuilder.TypeEnum |
NodesBetweenNodesBuilder.TypeEnum.NODE_AT_CENTER_OF_THREE_NODES
At the center of imaginary circle defined by 3 nodes
|
static NodesBetweenNodesBuilder.TypeEnum |
NodesBetweenNodesBuilder.TypeEnum.NODES_BETWEEN_TWO_NODES
Between two nodes
|
Modifier and Type | Method and Description |
---|---|
NodesBetweenNodesBuilder.TypeEnum |
NodesBetweenNodesBuilder.type()
Returns the node creation type
License requirements: None. |
static NodesBetweenNodesBuilder.TypeEnum |
NodesBetweenNodesBuilder.TypeEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodesBetweenNodesBuilder.TypeEnum |
NodesBetweenNodesBuilder.TypeEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodesBetweenNodesBuilder.TypeEnum[] |
NodesBetweenNodesBuilder.TypeEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NodesBetweenNodesBuilder.setType(NodesBetweenNodesBuilder.TypeEnum nodeCreationType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.