Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static NodeTranslateBuilder.CopyType |
NodeTranslateBuilder.CopyType.COPY_TRANSLATE
copy translate
|
static NodeTranslateBuilder.CopyType |
NodeTranslateBuilder.CopyType.TRANSLATE_ONLY
translate only
|
Modifier and Type | Method and Description |
---|---|
NodeTranslateBuilder.CopyType |
NodeTranslateBuilder.copyOption()
Returns the copy option
License requirements: None. |
static NodeTranslateBuilder.CopyType |
NodeTranslateBuilder.CopyType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodeTranslateBuilder.CopyType |
NodeTranslateBuilder.CopyType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodeTranslateBuilder.CopyType[] |
NodeTranslateBuilder.CopyType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NodeTranslateBuilder.setCopyOption(NodeTranslateBuilder.CopyType copyOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.