Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ModelUpdateSolution.TargetType |
ModelUpdateSolution.TargetType.ALL
Export all the targets to the csv file
|
static ModelUpdateSolution.TargetType |
ModelUpdateSolution.TargetType.FREQUENCIES
Export all the frequency targets to the csv file
|
static ModelUpdateSolution.TargetType |
ModelUpdateSolution.TargetType.MODE_SHAPES
Export all the mode shape targets to the csv file
|
Modifier and Type | Method and Description |
---|---|
static ModelUpdateSolution.TargetType |
ModelUpdateSolution.TargetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelUpdateSolution.TargetType |
ModelUpdateSolution.TargetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelUpdateSolution.TargetType[] |
ModelUpdateSolution.TargetType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelUpdateSolution.exportErrorsCsvFile(ModelUpdateSolution.TargetType targetType,
String fileName)
Export the model update errors to the csv file
License requirements: nx_correl_update ("FE Model Update") . |
void |
ModelUpdateSolution.exportTargetsCsvFile(ModelUpdateSolution.TargetType tagetType,
String fileName)
Export the model update targets to the csv file
License requirements: nx_correl_update ("FE Model Update") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.