Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ModelUpdateCorrelMethodBuilder.Method |
ModelUpdateCorrelMethodBuilder.Method.MAC
Correlation Method is MAC
|
static ModelUpdateCorrelMethodBuilder.Method |
ModelUpdateCorrelMethodBuilder.Method.XORTHO
Correlation Method is X_ORTHO
|
Modifier and Type | Method and Description |
---|---|
ModelUpdateCorrelMethodBuilder.Method |
ModelUpdateCorrelMethodBuilder.correlMethod()
Returns the correlation method
License requirements: None. |
static ModelUpdateCorrelMethodBuilder.Method |
ModelUpdateCorrelMethodBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelUpdateCorrelMethodBuilder.Method |
ModelUpdateCorrelMethodBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelUpdateCorrelMethodBuilder.Method[] |
ModelUpdateCorrelMethodBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelUpdateCorrelMethodBuilder.setCorrelMethod(ModelUpdateCorrelMethodBuilder.Method correlMethod)
License requirements: nx_correl_update ("FE Model Update") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.