Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MeshFromBoundaryBuilder.RailOption |
MeshFromBoundaryBuilder.RailOption.TRANSITION
transitioned layer
|
static MeshFromBoundaryBuilder.RailOption |
MeshFromBoundaryBuilder.RailOption.UNIFORM
single layer
|
Modifier and Type | Method and Description |
---|---|
MeshFromBoundaryBuilder.RailOption |
MeshFromBoundaryBuilder.railType()
Returns the type of rail mesh
License requirements: nx_masterfem ("Finite Element Modeling") . |
static MeshFromBoundaryBuilder.RailOption |
MeshFromBoundaryBuilder.RailOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshFromBoundaryBuilder.RailOption |
MeshFromBoundaryBuilder.RailOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshFromBoundaryBuilder.RailOption[] |
MeshFromBoundaryBuilder.RailOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeshFromBoundaryBuilder.setRailType(MeshFromBoundaryBuilder.RailOption option)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.