Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MeshFromBoundaryBuilder.LoopOption |
MeshFromBoundaryBuilder.LoopOption.CLOSED_LOOP
closed loop
|
static MeshFromBoundaryBuilder.LoopOption |
MeshFromBoundaryBuilder.LoopOption.SOURCE_TARGET
source target
|
Modifier and Type | Method and Description |
---|---|
MeshFromBoundaryBuilder.LoopOption |
MeshFromBoundaryBuilder.loopType()
Returns the type of loop
License requirements: nx_masterfem ("Finite Element Modeling") . |
static MeshFromBoundaryBuilder.LoopOption |
MeshFromBoundaryBuilder.LoopOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshFromBoundaryBuilder.LoopOption |
MeshFromBoundaryBuilder.LoopOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshFromBoundaryBuilder.LoopOption[] |
MeshFromBoundaryBuilder.LoopOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeshFromBoundaryBuilder.setLoopType(MeshFromBoundaryBuilder.LoopOption loopoption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.