Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MappedMeshBuilder.MidNodeType |
MappedMeshBuilder.MidNodeType.CURVED
Curved Option
|
static MappedMeshBuilder.MidNodeType |
MappedMeshBuilder.MidNodeType.MIXED
Mixed Option
|
static MappedMeshBuilder.MidNodeType |
MappedMeshBuilder.MidNodeType.STRAIGHT
Straight Option
|
Modifier and Type | Method and Description |
---|---|
MappedMeshBuilder.MidNodeType |
MappedMeshBuilder.midNodeOption()
Returns the mid node opt
License requirements: None. |
static MappedMeshBuilder.MidNodeType |
MappedMeshBuilder.MidNodeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MappedMeshBuilder.MidNodeType |
MappedMeshBuilder.MidNodeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MappedMeshBuilder.MidNodeType[] |
MappedMeshBuilder.MidNodeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MappedMeshBuilder.setMidNodeOption(MappedMeshBuilder.MidNodeType midNodeType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.