Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
ManualSweepBetweenListItemSelection |
ManualSweepBetweenSelection.createNewListItem(CAEEdge tMasterEdge,
CAEEdge tTargetEdge,
boolean fFlipDirection)
Deprecated.
Deprecated in NX10.0.0. Use
CAE.Mesh3dHexBuilder .
|
ManualSweepBetweenListItemSelection |
ManualSweepBetweenListItemSelectionList.findItem(int index)
Returns the object at the input index.
|
ManualSweepBetweenListItemSelection[] |
ManualSweepBetweenListItemSelectionList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ManualSweepBetweenListItemSelectionList.append(ManualSweepBetweenListItemSelection object)
Appends an object to the list
License requirements: None. |
void |
ManualSweepBetweenListItemSelectionList.append(ManualSweepBetweenListItemSelection[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ManualSweepBetweenListItemSelectionList.erase(ManualSweepBetweenListItemSelection obj)
Erases the object from the list, but does not delete the object.
|
void |
ManualSweepBetweenListItemSelectionList.erase(ManualSweepBetweenListItemSelection obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ManualSweepBetweenListItemSelectionList.findIndex(ManualSweepBetweenListItemSelection obj)
Finds the index where the input object appears.
|
void |
ManualSweepBetweenListItemSelectionList.insert(int location,
ManualSweepBetweenListItemSelection object)
Inserts an object at the specified location
License requirements: None. |
void |
ManualSweepBetweenListItemSelectionList.setContents(ManualSweepBetweenListItemSelection[] objects)
Sets the contents of the entire list.
|
void |
ManualSweepBetweenListItemSelectionList.swap(ManualSweepBetweenListItemSelection object1,
ManualSweepBetweenListItemSelection object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.