Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LocalRemeshBuilder.Option |
LocalRemeshBuilder.Option.FACTOR
Factor
|
static LocalRemeshBuilder.Option |
LocalRemeshBuilder.Option.SIZE
Absolute Size
|
Modifier and Type | Method and Description |
---|---|
LocalRemeshBuilder.Option |
LocalRemeshBuilder.sizeOption()
Returns the size option
License requirements: None. |
static LocalRemeshBuilder.Option |
LocalRemeshBuilder.Option.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LocalRemeshBuilder.Option |
LocalRemeshBuilder.Option.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LocalRemeshBuilder.Option[] |
LocalRemeshBuilder.Option.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LocalRemeshBuilder.setSizeOption(LocalRemeshBuilder.Option sizeOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.