Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum |
LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum.LINEAR
Linear increments
|
static LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum |
LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum.LOGARITHMIC
Logarithmic increments
|
Modifier and Type | Method and Description |
---|---|
LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum |
LaminateSineEventBuilder.intermediateFrequenciesBetweenOption()
Returns the intermediate in between frequencies option
License requirements: None. |
static LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum |
LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum |
LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum[] |
LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaminateSineEventBuilder.setIntermediateFrequenciesBetweenOption(LaminateSineEventBuilder.IntermediateFrequeciesBetweenEnum intermediateFrequenciesBetweenOption)
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.