Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CartesianCoordinateSystem
Represents a cartesian coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCoordinateSystem(nxopen.Point3d, nxopen.Matrix3x3, boolean) Created in NX4.0.0 |
interface |
CoordinateSystem
Represents a coordinate system
This is an abstract class . |
interface |
CylindricalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCylindricalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
PhysicalMaterial
Represents Physical Material .
|
interface |
SphericalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createSphericalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
Modifier and Type | Interface and Description | ||
---|---|---|---|
interface |
CaeRegion
Represents a cae region object
For more information, refer to the Solver language documentation
in the
interface DependentMesh
Represents Mesh Recipe
To create or edit an instance of this class, use DependentMeshBuilder Created in NX5.0.0 | ||
interface |
FEElement
Represents a Finite Element.
|
||
interface |
MappedMesh
Represents Mesh Recipe
To create or edit an instance of this class, use MappedMeshBuilder Created in NX5.0.0 |
||
interface |
Mesh
Represents a Mesh
For more information, refer to the Solver language documentation
in the
interface Mesh0d
Represents 0d Mesh
To create or edit an instance of this class, use Mesh0dBuilder Created in NX6.0.0 | ||
interface |
Mesh1d
Represents 1d Mesh
To create or edit an instance of this class, use Mesh1dBuilder Created in NX6.0.0 |
||
interface |
Mesh2d
Represents 2d Mesh
This is an abstract class . |
||
interface |
Mesh2dFree
Represents 2d Mesh
To create or edit an instance of this class, use Mesh2dBuilder Created in NX6.0.0 |
||
interface |
Mesh3d
Represents 3d Mesh
To create or edit an instance of this class, use Mesh3dTetBuilder Created in NX6.0.0 |
||
interface |
MeshFollower
Represents Mesh Recipe
This is an abstract class . |
||
interface |
MeshShellFromSolid
Represents 2d Mesh that follows 3d mesh
To create or edit an instance of this class, use SurfaceCoatBuilder Created in NX7.5.0 |
||
interface |
PrimitiveMesh
Represents Primitive Mesh
To create or edit an instance of this class, use PrimitiveMeshBuilder Created in NX7.5.0 |
||
interface |
SimBC
Represents BC class which is a superclass to
SimLoad and SimConstraint . |
||
interface |
SimConstraint
Represents a constraint
To create a new instance of this class, use SimConstraintCollection.createConstraint(java.lang.String, java.lang.String) Created in NX4.0.0 |
||
interface |
SimLoad
Represents a load
To create a new instance of this class, use SimLoadCollection.createLoad(java.lang.String, java.lang.String) Created in NX4.0.0 |
||
interface |
SimLoadSet
Represents a cae load set object
To create a new instance of this class, use SimLoadSetCollection.createLoadSet(java.lang.String, java.lang.String, int) Created in NX10.0.0 |
||
interface |
SimSimulationObject
Represents a simulation object
For more information, refer to the Solver language documentation
in the
interface SweptMesh
Represents swept Mesh
To create or edit an instance of this class, use Mesh3dHexBuilder Created in NX6.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.