Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FemPart.UseBodiesOption |
FemPart.UseBodiesOption.ALL_BODIES
Use all bodies from the cad part
|
static FemPart.UseBodiesOption |
FemPart.UseBodiesOption.SELECTED_BODIES
Use selected bodies from the cad part
|
FemPart.UseBodiesOption |
FemPart.GeometryData.useBodiesOption
Flag if all were selected
|
static FemPart.UseBodiesOption |
FemPart.UseBodiesOption.VISIBLE_BODIES
Use all visible bodies from the cad part
|
Modifier and Type | Method and Description |
---|---|
static FemPart.UseBodiesOption |
FemPart.UseBodiesOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FemPart.UseBodiesOption |
FemPart.UseBodiesOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FemPart.UseBodiesOption[] |
FemPart.UseBodiesOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FemPart.finalizeCreation(Part cadPart,
String idealizedPartName,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description)
Finalizes the creation of the fem part file.
|
void |
FemPart.finalizeCreation(Part cadPart,
String idealizedPartName,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description,
boolean isMorphEnabled)
Finalizes the creation of the fem part file.
|
void |
FemPart.finalizeCreation(Part cadPart,
String idealizedPartName,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
String[] description)
Deprecated.
Deprecated in NX9.0.0. Use
FemPart.finalizeCreation(nxopen.Part, java.lang.String, nxopen.cae.FemPart.UseBodiesOption, nxopen.Body[], nxopen.cae.FemSynchronizeOptions, java.lang.String, java.lang.String, java.lang.String[]) that includes abstraction type instead.
|
void |
FemPart.finalizeCreationManaged(Part cadPart,
boolean createIdealPart,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
BaseFemPart.AxisymAbstractionType abstractionType,
String[] description)
Finalizes the creation of the fem part file.
|
void |
FemPart.finalizeCreationManaged(Part cadPart,
boolean createIdealPart,
FemPart.UseBodiesOption useBodiesOption,
Body[] bodies,
FemSynchronizeOptions geometrySyncOptions,
String solverTypeName,
String analysisTypeType,
String[] description)
Deprecated.
Deprecated in NX9.0.0. Use
FemPart.finalizeCreationManaged(nxopen.Part, boolean, nxopen.cae.FemPart.UseBodiesOption, nxopen.Body[], nxopen.cae.FemSynchronizeOptions, java.lang.String, java.lang.String, nxopen.cae.BaseFemPart.AxisymAbstractionType, java.lang.String[]) that includes abstraction type instead.
|
void |
FemPart.setGeometryData(FemPart.UseBodiesOption useBodiesOption,
Body[] listOfBodies,
FemSynchronizeOptions psyncData)
Sets the geometry data associated with the fem part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.