Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.modelcheck |
Provides classes and interfaces for Model Check.
|
Modifier and Type | Field and Description |
---|---|
FEElemEdge[] |
ElemEdgePathMethod.PathEdgesData.pathelemedges
resultant element edges
|
FEElemEdge[] |
ElemEdgePathMethod.SeedEdgesData.seedelemedges
seed element edges
|
FEElemEdge[] |
ElemEdgePathMethod.SeedsData.seedelemedges
seed element edges
|
Modifier and Type | Method and Description |
---|---|
void |
ElemEdgePathMethod.addSeedEdge(FENode seedStartNode,
FEElemEdge seedElemEdge)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
ElemEdgePathMethod.addSeedEdge(FENode, nxopen.cae.FEElemEdge) with additional arguments instead.
|
void |
ElemEdgePathMethod.addSeedEdge(FENode seedStartNode,
FEElemEdge seedElemEdge,
boolean preferFreeEdges,
boolean preferGeometryAssociatedEdges,
boolean preferFeatureElementEdge,
double featureAngleTolerance,
boolean allowGapJumping,
double gapJumpingTolerance)
Add seed (start vertex and edge) to the end of the path.
|
ElemEdgePathMethod |
SmartSelectionManager.createElemEdgePathMethod(FEElemEdge seedElemEdgeTag,
FENode seedStartNodeTag)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
SmartSelectionManager.createElemEdgePathMethod(nxopen.cae.FEElemEdge, FENode) with additional arguments instead.
|
ElemEdgePathMethod |
SmartSelectionManager.createElemEdgePathMethod(FEElemEdge seedElemEdgeTag,
FENode seedStartNodeTag,
boolean preferFreeEdges,
boolean preferGeometryAssociatedEdges,
boolean preferFeatureElementEdge,
double featureAngleTolerance,
boolean allowGapJumping,
double gapJumpingTolerance)
Creates an elem edge path method
License requirements: nx_masterfem ("Finite Element Modeling") . |
FeatureEdgeNodeMethod |
SmartSelectionManager.createFeatureEdgeNodeMethod(FEElemEdge[] seedTags,
double dFeatureAngle)
Creates a feature edge node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
FeatureElemEdgeMethod |
SmartSelectionManager.createFeatureElemEdgeMethod(FEElemEdge[] seedTags,
double dFeatureAngle)
Creates a feature elem edge method
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
ElemEdgePathMethod.removeSeedEdge(FEElemEdge seedElemEdge)
Remove seed (start vertex and edge) from the path.
|
void |
SimBcXyPlotBuilder.setLocationElementEdge(FEElemEdge elementEdge)
Sets location at an element edge
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SetManager.setTargetSetElemEdgePath(int setIndex,
FEElemEdge[] seedEdges,
FENode[] seedVertices)
Deprecated.
Deprecated in NX10.0.0. Use overloaded
CAE.SetManager#setTargetSetElemEdgePath with additional arguments instead.
|
void |
SetManager.setTargetSetElemEdgePath(int setIndex,
FEElemEdge[] seedEdges,
FENode[] seedVertices,
boolean[] preferFreeEdges,
boolean[] preferGeometryAssociatedEdges,
boolean[] preferFeatureElementEdges,
double[] featureAngleTolerance,
boolean[] allowGapJumping,
double[] gapJumpingTolerance)
Sets the CAE element edge path in the specified set
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Field and Description |
---|---|
FEElemEdge[] |
ElementEdgeCheckBuilder.ExecuteCheckData.freeedges
free element edges
|
FEElemEdge[] |
ElementEdgeCheckBuilder.ExecuteCheckData.nonmanifoldedges
non-manifold element edges
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.