Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.ElemDimensionType.ANY
any element can be selected
|
static ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.ElemDimensionType.BEAM
only beam elements can be selected
|
static ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.ElemDimensionType.SHELL
only shell elements can be selected
|
static ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.ElemDimensionType.SOLID
only solid elements can be selected
|
Modifier and Type | Method and Description |
---|---|
ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.elementDimension()
Returns the dimension of the elements to be translated
License requirements: None. |
static ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.ElemDimensionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementTranslateBuilder.ElemDimensionType |
ElementTranslateBuilder.ElemDimensionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementTranslateBuilder.ElemDimensionType[] |
ElementTranslateBuilder.ElemDimensionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementTranslateBuilder.setElementDimension(ElementTranslateBuilder.ElemDimensionType elementDimension)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.