Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.SplitMethodType.ELEMENT_SHAPE
Based on element shape
|
static ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.SplitMethodType.EXISTING_CONNECTIVITY
use existing element connectivity
|
static ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.SplitMethodType.INTERACTIVE_MOUSE_LOCATION
Interactive Element Split
|
static ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.SplitMethodType.SEED_ELEMENT
by vector comparison
|
Modifier and Type | Method and Description |
---|---|
ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.splitMethod()
Returns the use existing connectivity option
License requirements: nx_masterfem ("Finite Element Modeling") . |
static ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.SplitMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementSplitBuilder.SplitMethodType |
ElementSplitBuilder.SplitMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementSplitBuilder.SplitMethodType[] |
ElementSplitBuilder.SplitMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementSplitBuilder.setSplitMethod(ElementSplitBuilder.SplitMethodType option)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.