Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementConnectivityBuilder.Types |
ElementConnectivityBuilder.Types.ALL_ELEMENTS_ATTACHED_TO_NODE
Modify connectivities of all attached elements to nodes.
|
static ElementConnectivityBuilder.Types |
ElementConnectivityBuilder.Types.SINGLE_ELEMENT
Modify connectivity of selected element.
|
Modifier and Type | Method and Description |
---|---|
ElementConnectivityBuilder.Types |
ElementConnectivityBuilder.type()
Returns a type which indicates whether connectivity is to be modfied for selected element or all attached elements.
|
static ElementConnectivityBuilder.Types |
ElementConnectivityBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementConnectivityBuilder.Types |
ElementConnectivityBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementConnectivityBuilder.Types[] |
ElementConnectivityBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementConnectivityBuilder.setType(ElementConnectivityBuilder.Types type)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.