Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementConnectivityBuilder.Methods |
ElementConnectivityBuilder.Methods.MODIFY_LEGS
Add or delete leg nodes of spider element
|
static ElementConnectivityBuilder.Methods |
ElementConnectivityBuilder.Methods.REPLACE_NODE
Replace a node of an element by another one
|
static ElementConnectivityBuilder.Methods |
ElementConnectivityBuilder.Methods.SWAP_ENDS
Swap the nodes of a 2-noded element
|
Modifier and Type | Method and Description |
---|---|
ElementConnectivityBuilder.Methods |
ElementConnectivityBuilder.method()
Returns an element modification method.
|
static ElementConnectivityBuilder.Methods |
ElementConnectivityBuilder.Methods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementConnectivityBuilder.Methods |
ElementConnectivityBuilder.Methods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementConnectivityBuilder.Methods[] |
ElementConnectivityBuilder.Methods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementConnectivityBuilder.setMethod(ElementConnectivityBuilder.Methods method)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.