Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ModelUpdateSolution
Represents a
ModelUpdateSolution , which is a meta-solution used to update finite element models to match real life test data To create or edit an instance of this class, use ModelUpdateSolutionBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
CorrelSolution |
CorrelSolutionCollection.activeSolution()
Returns the active solution
License requirements: None. |
CorrelSolution |
CorrelSolution.cloneCorrelation()
Make a clone of a correl solution.
|
CorrelSolution |
CorrelSolutionCollection.cloneSolution(CorrelSolution oldSolution,
String suggestedName)
Clones a correl meta solution
License requirements: None. |
CorrelSolution |
CorrelSolutionCollection.findObject(String solutionName)
Finds a correl meta solution with specified solution name
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
CorrelSolution |
CorrelSolutionCollection.cloneSolution(CorrelSolution oldSolution,
String suggestedName)
Clones a correl meta solution
License requirements: None. |
ShapeMetricViewerBuilder |
CorrelSolutionCollection.createShapeMetricViewerBuilder(CorrelSolution solution)
Creates the builder object of correl shape metric viewer
License requirements: nx_correl_base ("FE Correlation") . |
CorrelSolutionBuilder |
CorrelSolutionCollection.createSolutionBuilder(CorrelSolution solution)
Creates the builder object of correl meta solution
License requirements: None. |
void |
ComacViewerBuilder.init(CorrelSolution solution,
double[] comacsValues,
int[] nodeIndex,
int[] dofIndex)
Access the reference modes
License requirements: nx_correl_base ("FE Correlation") . |
void |
CorrelSolutionCollection.setActiveSolution(CorrelSolution activeSolution)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.