Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.NEG_XC |
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.NEG_YC |
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.NEG_ZC |
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.XC |
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.YC |
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.ZC |
Modifier and Type | Method and Description |
---|---|
CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.angleEnum()
Returns the angle vector enumeration
License requirements: None. |
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CorrelFineTuneAlignmentBuilder.AngleVector |
CorrelFineTuneAlignmentBuilder.AngleVector.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CorrelFineTuneAlignmentBuilder.AngleVector[] |
CorrelFineTuneAlignmentBuilder.AngleVector.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CorrelFineTuneAlignmentBuilder.setAngleEnum(CorrelFineTuneAlignmentBuilder.AngleVector angleEnum)
License requirements: nx_correl_base ("FE Correlation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.