Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CorrelAlignmentBuilder
This builder is used to control the alignment parameters of a
CorrelSolution To create a new instance of this class, use SimSolution.createAlignmentBuilder() Created in NX6.0.1 |
interface |
CorrelApplyAlignmentFromBuilder
This builder is used to apply the alignment matrix read from selected xml file to the test model
To create a new instance of this class, use CorrelManager.createCorrelApplyAlignmentFromBuilder(nxopen.cae.SimSolution) Created in NX9.0.0 |
interface |
CorrelFineTuneAlignmentBuilder
This builder is used to nudge the alignment by a fine adjustment
To create a new instance of this class, use CorrelManager.createCorrelFineTuneAlignmentBuilder(nxopen.cae.SimSolution) Created in NX9.0.0 |
interface |
CorrelModePairingBuilder
This builder is used to control the mode pairing behavior of a
CorrelSolution To create a new instance of this class, use CorrelSolution.createModePairingBuilder() Created in NX6.0.1 |
interface |
CorrelSolutionBuilder
This is a manager to the
CAE.CorrelSolution class. |
interface |
ModelUpdateSolutionBuilder
Represents a
ModelUpdateSolutionBuilder To create a new instance of this class, use ModelUpdateSolutionCollection.createSolutionBuilder(nxopen.cae.ModelUpdateSolution) Created in NX7.5.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.