Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CorrelAlignmentBuilder.ScalingChoice |
CorrelAlignmentBuilder.ScalingChoice.FROM_SECOND_AXIS
Computed from the lenght of the second axis
|
static CorrelAlignmentBuilder.ScalingChoice |
CorrelAlignmentBuilder.ScalingChoice.SPECIFY
User specified scaling factor
|
Modifier and Type | Method and Description |
---|---|
CorrelAlignmentBuilder.ScalingChoice |
CorrelAlignmentBuilder.scalingType()
Returns the scaling type
License requirements: None. |
static CorrelAlignmentBuilder.ScalingChoice |
CorrelAlignmentBuilder.ScalingChoice.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CorrelAlignmentBuilder.ScalingChoice |
CorrelAlignmentBuilder.ScalingChoice.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CorrelAlignmentBuilder.ScalingChoice[] |
CorrelAlignmentBuilder.ScalingChoice.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CorrelAlignmentBuilder.setScalingType(CorrelAlignmentBuilder.ScalingChoice scalingType)
License requirements: nx_correl_base ("FE Correlation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.