Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.FIVE |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.FOUR |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.ONE |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.THREE |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.TWO |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.ZERO |
Modifier and Type | Method and Description |
---|---|
CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.localSubdivision()
Returns the local subdivision
License requirements: None. |
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CfdContactPreventionConstraintBuilder.LocalSubdivisions |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CfdContactPreventionConstraintBuilder.LocalSubdivisions[] |
CfdContactPreventionConstraintBuilder.LocalSubdivisions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CfdContactPreventionConstraintBuilder.setLocalSubdivision(CfdContactPreventionConstraintBuilder.LocalSubdivisions localSubdivision)
License requirements: nx_adv_fluid_mod ("NX Advanced Fluid Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.