Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CaeSetObjectSubType |
CaeSetObjectSubType.ELEMENT_EDGE
sub type is element edge
|
static CaeSetObjectSubType |
CaeSetObjectSubType.ELEMENT_FACE
sub type is element face
|
static CaeSetObjectSubType |
CaeSetObjectSubType.NONE
sub type is the same as the type of the object
|
static CaeSetObjectSubType |
CaeSetObjectSubType.PART
sub type is part, used for Gravity Loads
|
CaeSetObjectSubType |
SetObject.subType
object sub_component type
|
Modifier and Type | Method and Description |
---|---|
static CaeSetObjectSubType |
CaeSetObjectSubType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeSetObjectSubType |
CaeSetObjectSubType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeSetObjectSubType[] |
CaeSetObjectSubType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
SetObject(TaggedObject objInitial,
CaeSetObjectSubType subTypeInitial,
int subIdInitial)
Constructor for the SetObject object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.