public static class WeldBuilder.NumberOfPointsOnEdgeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM_NUMBER
Create the maximum number of points on an edge
|
static int |
_SPECIFIED_NUMBER
Specify the number of points to be created on an edge
|
static WeldBuilder.NumberOfPointsOnEdgeType |
MAXIMUM_NUMBER
Create the maximum number of points on an edge
|
static WeldBuilder.NumberOfPointsOnEdgeType |
SPECIFIED_NUMBER
Specify the number of points to be created on an edge
|
Modifier and Type | Method and Description |
---|---|
static WeldBuilder.NumberOfPointsOnEdgeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBuilder.NumberOfPointsOnEdgeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBuilder.NumberOfPointsOnEdgeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldBuilder.NumberOfPointsOnEdgeType MAXIMUM_NUMBER
public static final WeldBuilder.NumberOfPointsOnEdgeType SPECIFIED_NUMBER
public static final int _MAXIMUM_NUMBER
public static final int _SPECIFIED_NUMBER
public static WeldBuilder.NumberOfPointsOnEdgeType valueOf(int value)
public static WeldBuilder.NumberOfPointsOnEdgeType valueOf(String name)
public static WeldBuilder.NumberOfPointsOnEdgeType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.