public static class SimSolution.SolveOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EDIT_SOLVER_INPUT_FILE
edit existing solver input file
|
static int |
_SOLVE
write solver input file and launch solve
|
static int |
_SOLVE_INPUT_FILE
launch solve with existing solver input file
|
static int |
_WRITE_EDIT_AND_SOLVE_INPUT_FILE
write solver input file, allow edit and then launch solve
|
static int |
_WRITE_SOLVER_INPUT_FILE
write solver input file only
|
static SimSolution.SolveOption |
EDIT_SOLVER_INPUT_FILE
edit existing solver input file
|
static SimSolution.SolveOption |
SOLVE
write solver input file and launch solve
|
static SimSolution.SolveOption |
SOLVE_INPUT_FILE
launch solve with existing solver input file
|
static SimSolution.SolveOption |
WRITE_EDIT_AND_SOLVE_INPUT_FILE
write solver input file, allow edit and then launch solve
|
static SimSolution.SolveOption |
WRITE_SOLVER_INPUT_FILE
write solver input file only
|
Modifier and Type | Method and Description |
---|---|
static SimSolution.SolveOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimSolution.SolveOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimSolution.SolveOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimSolution.SolveOption SOLVE
public static final SimSolution.SolveOption WRITE_SOLVER_INPUT_FILE
public static final SimSolution.SolveOption SOLVE_INPUT_FILE
public static final SimSolution.SolveOption WRITE_EDIT_AND_SOLVE_INPUT_FILE
public static final SimSolution.SolveOption EDIT_SOLVER_INPUT_FILE
public static final int _SOLVE
public static final int _WRITE_SOLVER_INPUT_FILE
public static final int _SOLVE_INPUT_FILE
public static final int _WRITE_EDIT_AND_SOLVE_INPUT_FILE
public static final int _EDIT_SOLVER_INPUT_FILE
public static SimSolution.SolveOption valueOf(int value)
public static SimSolution.SolveOption valueOf(String name)
public static SimSolution.SolveOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.