public interface SimPart extends CaePart
PartCollection
class to load or create a part. Modifier and Type | Interface and Description |
---|---|
static class |
SimPart.ImportErrorCodes
Contains list of error codes for import of each entity type
|
static class |
SimPart.ImportOptions
Contains information about which entities to be imported
|
BasePart.BookmarkOption, BasePart.CloseAfterSave, BasePart.CloseModified, BasePart.CloseWholeTree, BasePart.CollaborativeContentType, BasePart.HistoryEventInformation, BasePart.IncompleteStatus, BasePart.PartPreview, BasePart.PreviewImageData, BasePart.ReopenData, BasePart.SaveComponents, BasePart.TransientStatus, BasePart.Units
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat
Modifier and Type | Method and Description |
---|---|
CaePart |
femPart()
Returns the fem part associated with the sim part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
finalizeCreation(CaePart femPart,
int femLayerOpt,
String[] description)
Finalizes the creation of the sim part file.
|
void |
finalizeCreation(CaePart femPart,
String[] description)
Finalizes the creation of the sim part file.
|
SimPart.ImportErrorCodes |
importSim(String fileName,
String prependString,
SimPart.ImportOptions selOptions,
FEModelOccurrence[] selectedFemoccs)
Imports selected entities from the source sim into the current (target) sim.
|
SimSimulation |
simulation()
Returns the
SimSimulation object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX4.0.0 |
caeGroups, createModelDisplayBuilder, createSolverAppendOption, deleteSolverAppendOption, elementQualitySettings, exportJt, exportSimulation, getCsysFlattenedLabel, getDescription, importExistingSimulation, meshControlDisplayMgr, modelCheckMgr, modelingObjectPropertyTables, newBeamSectionOffsetOptions, newBeamSectionOptions, newBeamSectionOrientationOptions, newMaterialOptions, nodeElementInfoMgr, physicalPropertyTables, selectElementMgr, setDescription, showHideMgr, smartSelectionMgr
analysisManager, arcs, assemblies, assemblyManager, assignPermanentName, axes, baseFeatures, cameras, camfeatures, canBeDisplayPart, cgfxAttrs, cgfxMattex, close, colors, completeStructure, componentAssembly, coordinateSystems, createDynamicSectionBuilder, createEffectivityConditionBuilder, createEffectivityConditionBuilder, createFacetSettingsBuilder, createGatewayGroupBuilder, createPerspectiveOptionsBuilder, createReferenceSet, curves, datums, decals, deleteReferenceSet, designStudy, directions, dynamicSections, ellipses, expressionGroups, expressions, fieldManager, fonts, fullPath, functions, getAllReferenceSets, getCollaborativeContentType, getHistoryInformation, getIncompleteStatus, getMakeUniqueName, getPreviewImage, getTransientStatus, grids, hyperbolas, imageCaptureManager, images, imagesData, infiniteLines, isFullyLoaded, isReadOnly, layerCategories, layers, layouts, leaf, lights, lines, loadFeatureDataForSelection, loadFully, loadThisPartFully, materialManager, measureManager, modelingViews, nxmatrices, offsets, optimization, parabolas, partPreviewMode, partUnits, pdmpart, planes, plotManager, points, polylines, preferences, propertiesManager, regenerateDisplayFacets, reinstateTransience, removeTransience, reopen, reopenAs, requirementChecks, requirements, reverseBlankAll, ruleManager, save, saveAs, saveBookmark, saveDisplayFacets, saveOptions, scalars, scCollectors, sections, selPref, setMakeUniqueName, setPartPreviewMode, setSaveDisplayFacets, setUniqueIdentifier, shedobjs, splines, trueStudioObjs, uniqueIdentifier, unitCollection, userDefinedObjectManager, validations, views, wcs, xforms
deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
SimSimulation simulation() throws NXException, RemoteException
SimSimulation
object
SimSimulation
NXException
RemoteException
void finalizeCreation(CaePart femPart, String[] description) throws NXException, RemoteException
femPart
- the fem part file FemPart
description
- description NXException
RemoteException
void finalizeCreation(CaePart femPart, int femLayerOpt, String[] description) throws NXException, RemoteException
femPart
- the fem part file FemPart
femLayerOpt
- layer option. -1 = USE_ORIGINAL, 0 = USE_WORKdescription
- description NXException
RemoteException
CaePart femPart() throws NXException, RemoteException
NXException
RemoteException
SimPart.ImportErrorCodes importSim(String fileName, String prependString, SimPart.ImportOptions selOptions, FEModelOccurrence[] selectedFemoccs) throws NXException, RemoteException
fileName
- name of the source simulation file prependString
- string to prepend imported simulation entity names, can be NULL or empty selOptions
- options indicating the types of entities to be importedselectedFemoccs
- Array of FeModelOccurrences to import onto FEModelOccurrence
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.