public static class SimBcXyPlotBuilder.ResolveMultipleMatches extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD |
static int |
_AVERAGE |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_MULTIPLE_CURVES |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
ADD |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
AVERAGE |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
MAXIMUM |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
MINIMUM |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
MULTIPLE_CURVES |
Modifier and Type | Method and Description |
---|---|
static SimBcXyPlotBuilder.ResolveMultipleMatches |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimBcXyPlotBuilder.ResolveMultipleMatches |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimBcXyPlotBuilder.ResolveMultipleMatches[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimBcXyPlotBuilder.ResolveMultipleMatches ADD
public static final SimBcXyPlotBuilder.ResolveMultipleMatches AVERAGE
public static final SimBcXyPlotBuilder.ResolveMultipleMatches MINIMUM
public static final SimBcXyPlotBuilder.ResolveMultipleMatches MAXIMUM
public static final SimBcXyPlotBuilder.ResolveMultipleMatches MULTIPLE_CURVES
public static final int _ADD
public static final int _AVERAGE
public static final int _MINIMUM
public static final int _MAXIMUM
public static final int _MULTIPLE_CURVES
public static SimBcXyPlotBuilder.ResolveMultipleMatches valueOf(int value)
public static SimBcXyPlotBuilder.ResolveMultipleMatches valueOf(String name)
public static SimBcXyPlotBuilder.ResolveMultipleMatches[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.