Modifier and Type | Method and Description |
---|---|
ShowAdjacentBuilder |
createShowAdjacentBuilder()
Creates a builder for Show Adjacent Command
License requirements: nx_masterfem ("Finite Element Modeling") . |
ShowHideBuilder |
createShowHideBuilder()
Creates a builder for Show Hide Command
License requirements: nx_masterfem ("Finite Element Modeling") . |
ShowOnlyBuilder |
createShowOnlyBuilder()
Creates a builder for Show Only Command
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
reverseFaceDisplay()
Creates a builder for the Reverse Face Display Command, which reverses the display of
each CAE geometry face in the model.
|
ShowAdjacentBuilder createShowAdjacentBuilder() throws NXException, RemoteException
NXException
RemoteException
ShowOnlyBuilder createShowOnlyBuilder() throws NXException, RemoteException
NXException
RemoteException
ShowHideBuilder createShowHideBuilder() throws NXException, RemoteException
NXException
RemoteException
void reverseFaceDisplay() throws NXException, RemoteException
#ja_SHOW_HIDE_MANAGER_create_show_only_builder
to examine the CAE
model visually. For example, use the show only to visually check the a BC's target
sets, and then use reverse face display to visually examine the CAE geometry which
doesn't have this BC defined on it.
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.