public static class ShellEADBuilder.MaterialOrientationMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COORDINATE_SYSTEM
use a coordinate system to orient the material
|
static int |
_VECTOR_PROJECTION
use a vector projected to the shell to orient the material
|
static ShellEADBuilder.MaterialOrientationMethod |
COORDINATE_SYSTEM
use a coordinate system to orient the material
|
static ShellEADBuilder.MaterialOrientationMethod |
VECTOR_PROJECTION
use a vector projected to the shell to orient the material
|
Modifier and Type | Method and Description |
---|---|
static ShellEADBuilder.MaterialOrientationMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellEADBuilder.MaterialOrientationMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellEADBuilder.MaterialOrientationMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShellEADBuilder.MaterialOrientationMethod COORDINATE_SYSTEM
public static final ShellEADBuilder.MaterialOrientationMethod VECTOR_PROJECTION
public static final int _COORDINATE_SYSTEM
public static final int _VECTOR_PROJECTION
public static ShellEADBuilder.MaterialOrientationMethod valueOf(int value)
public static ShellEADBuilder.MaterialOrientationMethod valueOf(String name)
public static ShellEADBuilder.MaterialOrientationMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.