public static class ResultsManipulationBuilder.ElementValueAtNode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AVERAGE |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static int |
_SUM |
static ResultsManipulationBuilder.ElementValueAtNode |
AVERAGE |
static ResultsManipulationBuilder.ElementValueAtNode |
MAXIMUM |
static ResultsManipulationBuilder.ElementValueAtNode |
MINIMUM |
static ResultsManipulationBuilder.ElementValueAtNode |
SUM |
Modifier and Type | Method and Description |
---|---|
static ResultsManipulationBuilder.ElementValueAtNode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultsManipulationBuilder.ElementValueAtNode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultsManipulationBuilder.ElementValueAtNode[] |
values()
Returns an array that contains the values for this enum.
|
public static final ResultsManipulationBuilder.ElementValueAtNode AVERAGE
public static final ResultsManipulationBuilder.ElementValueAtNode MAXIMUM
public static final ResultsManipulationBuilder.ElementValueAtNode MINIMUM
public static final ResultsManipulationBuilder.ElementValueAtNode SUM
public static final int _AVERAGE
public static final int _MAXIMUM
public static final int _MINIMUM
public static final int _SUM
public static ResultsManipulationBuilder.ElementValueAtNode valueOf(int value)
public static ResultsManipulationBuilder.ElementValueAtNode valueOf(String name)
public static ResultsManipulationBuilder.ElementValueAtNode[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.