public static class PostGraphBuilder.EntityType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BODY |
static int |
_EDGE |
static int |
_ELEMENT |
static int |
_FACE |
static int |
_NODE |
static int |
_POINT |
static PostGraphBuilder.EntityType |
BODY |
static PostGraphBuilder.EntityType |
EDGE |
static PostGraphBuilder.EntityType |
ELEMENT |
static PostGraphBuilder.EntityType |
FACE |
static PostGraphBuilder.EntityType |
NODE |
static PostGraphBuilder.EntityType |
POINT |
Modifier and Type | Method and Description |
---|---|
static PostGraphBuilder.EntityType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.EntityType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.EntityType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PostGraphBuilder.EntityType NODE
public static final PostGraphBuilder.EntityType ELEMENT
public static final PostGraphBuilder.EntityType POINT
public static final PostGraphBuilder.EntityType EDGE
public static final PostGraphBuilder.EntityType FACE
public static final PostGraphBuilder.EntityType BODY
public static final int _NODE
public static final int _ELEMENT
public static final int _POINT
public static final int _EDGE
public static final int _FACE
public static final int _BODY
public static PostGraphBuilder.EntityType valueOf(int value)
public static PostGraphBuilder.EntityType valueOf(String name)
public static PostGraphBuilder.EntityType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.