public static class Post.ValueSharingCriterion extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AVERAGE |
static int |
_MAXIMUM |
static int |
_MINIMUM |
static Post.ValueSharingCriterion |
AVERAGE |
static Post.ValueSharingCriterion |
MAXIMUM |
static Post.ValueSharingCriterion |
MINIMUM |
Modifier and Type | Method and Description |
---|---|
static Post.ValueSharingCriterion |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.ValueSharingCriterion |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.ValueSharingCriterion[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.ValueSharingCriterion AVERAGE
public static final Post.ValueSharingCriterion MINIMUM
public static final Post.ValueSharingCriterion MAXIMUM
public static final int _AVERAGE
public static final int _MINIMUM
public static final int _MAXIMUM
public static Post.ValueSharingCriterion valueOf(int value)
public static Post.ValueSharingCriterion valueOf(String name)
public static Post.ValueSharingCriterion[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.