public static class Post.Threshold extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISPLAYED |
static int |
_RESULT |
static int |
_SPECIFIED |
static int |
_VIEWPORT_DISPLAYED |
static int |
_VIEWPORT_RESULT |
static Post.Threshold |
DISPLAYED |
static Post.Threshold |
RESULT |
static Post.Threshold |
SPECIFIED |
static Post.Threshold |
VIEWPORT_DISPLAYED |
static Post.Threshold |
VIEWPORT_RESULT |
Modifier and Type | Method and Description |
---|---|
static Post.Threshold |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Threshold |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Threshold[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.Threshold RESULT
public static final Post.Threshold DISPLAYED
public static final Post.Threshold SPECIFIED
public static final Post.Threshold VIEWPORT_RESULT
public static final Post.Threshold VIEWPORT_DISPLAYED
public static final int _RESULT
public static final int _DISPLAYED
public static final int _SPECIFIED
public static final int _VIEWPORT_RESULT
public static final int _VIEWPORT_DISPLAYED
public static Post.Threshold valueOf(int value)
public static Post.Threshold valueOf(String name)
public static Post.Threshold[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.