public static class Post.ResultForPostviewData extends Object implements Serializable
Post.getResultForPostview(int)
Modifier and Type | Field and Description |
---|---|
Result |
result
Result which defines input postview |
ResultParameters |
resultParamter
a copy of the
ResultParameters which defines input postview, It is user's responsibility to destroy the result parameters object once done
using ResultManager.deleteResultParameters(nxopen.cae.ResultParameters) , in order to free up system resources |
Constructor and Description |
---|
ResultForPostviewData() |
public ResultParameters resultParamter
ResultParameters
which defines input postview, It is user's responsibility to destroy the result parameters object once done
using ResultManager.deleteResultParameters(nxopen.cae.ResultParameters)
, in order to free up system resourcesCopyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.