public static class MeshFromBoundaryBuilder.LoopOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CLOSED_LOOP
closed loop
|
static int |
_SOURCE_TARGET
source target
|
static MeshFromBoundaryBuilder.LoopOption |
CLOSED_LOOP
closed loop
|
static MeshFromBoundaryBuilder.LoopOption |
SOURCE_TARGET
source target
|
Modifier and Type | Method and Description |
---|---|
static MeshFromBoundaryBuilder.LoopOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshFromBoundaryBuilder.LoopOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshFromBoundaryBuilder.LoopOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final MeshFromBoundaryBuilder.LoopOption SOURCE_TARGET
public static final MeshFromBoundaryBuilder.LoopOption CLOSED_LOOP
public static final int _SOURCE_TARGET
public static final int _CLOSED_LOOP
public static MeshFromBoundaryBuilder.LoopOption valueOf(int value)
public static MeshFromBoundaryBuilder.LoopOption valueOf(String name)
public static MeshFromBoundaryBuilder.LoopOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.