public static class MeshControlBuilder.WeldSide extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOTH |
static int |
_SIDE1 |
static int |
_SIDE2 |
static MeshControlBuilder.WeldSide |
BOTH |
static MeshControlBuilder.WeldSide |
SIDE1 |
static MeshControlBuilder.WeldSide |
SIDE2 |
Modifier and Type | Method and Description |
---|---|
static MeshControlBuilder.WeldSide |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshControlBuilder.WeldSide |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshControlBuilder.WeldSide[] |
values()
Returns an array that contains the values for this enum.
|
public static final MeshControlBuilder.WeldSide BOTH
public static final MeshControlBuilder.WeldSide SIDE1
public static final MeshControlBuilder.WeldSide SIDE2
public static final int _BOTH
public static final int _SIDE1
public static final int _SIDE2
public static MeshControlBuilder.WeldSide valueOf(int value)
public static MeshControlBuilder.WeldSide valueOf(String name)
public static MeshControlBuilder.WeldSide[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.