public static class MechanicalLoadSumBuilder.UserUnit extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DECK_UNIT
Load unit = same as Solver Deck Unit
|
static int |
_FT_POUND_FORCE
Load unit = "lbf", Moment unit lbf-ft
|
static int |
_IN_POUND_FORCE
Load unit = "lbf", Moment unit lbf-in
|
static int |
_METER_NEWTON
Load unit = "N", Moment unit N-m
|
static int |
_MILLI_MILLINEWTON
Load unit = "mN", Moment unit N-mm
|
static int |
_MILLI_NEWTON
Load unit = "N", Moment unit N-mm
|
static MechanicalLoadSumBuilder.UserUnit |
DECK_UNIT
Load unit = same as Solver Deck Unit
|
static MechanicalLoadSumBuilder.UserUnit |
FT_POUND_FORCE
Load unit = "lbf", Moment unit lbf-ft
|
static MechanicalLoadSumBuilder.UserUnit |
IN_POUND_FORCE
Load unit = "lbf", Moment unit lbf-in
|
static MechanicalLoadSumBuilder.UserUnit |
METER_NEWTON
Load unit = "N", Moment unit N-m
|
static MechanicalLoadSumBuilder.UserUnit |
MILLI_MILLINEWTON
Load unit = "mN", Moment unit N-mm
|
static MechanicalLoadSumBuilder.UserUnit |
MILLI_NEWTON
Load unit = "N", Moment unit N-mm
|
Modifier and Type | Method and Description |
---|---|
static MechanicalLoadSumBuilder.UserUnit |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MechanicalLoadSumBuilder.UserUnit |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MechanicalLoadSumBuilder.UserUnit[] |
values()
Returns an array that contains the values for this enum.
|
public static final MechanicalLoadSumBuilder.UserUnit DECK_UNIT
public static final MechanicalLoadSumBuilder.UserUnit MILLI_NEWTON
public static final MechanicalLoadSumBuilder.UserUnit MILLI_MILLINEWTON
public static final MechanicalLoadSumBuilder.UserUnit METER_NEWTON
public static final MechanicalLoadSumBuilder.UserUnit FT_POUND_FORCE
public static final MechanicalLoadSumBuilder.UserUnit IN_POUND_FORCE
public static final int _DECK_UNIT
public static final int _MILLI_NEWTON
public static final int _MILLI_MILLINEWTON
public static final int _METER_NEWTON
public static final int _FT_POUND_FORCE
public static final int _IN_POUND_FORCE
public static MechanicalLoadSumBuilder.UserUnit valueOf(int value)
public static MechanicalLoadSumBuilder.UserUnit valueOf(String name)
public static MechanicalLoadSumBuilder.UserUnit[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.