public static class FEModel.IdSpecificationObject extends Object implements Serializable
CAE.FEModel#appendFemodel
Modifier and Type | Field and Description |
---|---|
boolean |
elementIdOffset
If true element_start_id will be used as an offset for imported element ids
|
int |
elementStartId
Start id to use for imported elements
|
String |
femObjectPrependName
String to prepend to fem object names such as element collector, material and section
|
boolean |
nodeIdOffset
If true node_start_id will be used as an offset for imported node ids
|
int |
nodeStartId
Start id to use for imported nodes
|
boolean |
physicalPropertyTableIdOffset
If true physical_property_table_start_id will be used as an offset for imported physical property table ids
|
int |
physicalPropertyTableStartId
Start id to use for imported physical property tables
|
Constructor and Description |
---|
IdSpecificationObject() |
IdSpecificationObject(String femObjectPrependNameInitial,
int nodeStartIdInitial,
boolean nodeIdOffsetInitial,
int elementStartIdInitial,
boolean elementIdOffsetInitial,
int physicalPropertyTableStartIdInitial,
boolean physicalPropertyTableIdOffsetInitial)
Constructor for the IdSpecificationObject object.
|
public String femObjectPrependName
public int nodeStartId
public boolean nodeIdOffset
public int elementStartId
public boolean elementIdOffset
public int physicalPropertyTableStartId
public boolean physicalPropertyTableIdOffset
public IdSpecificationObject()
public IdSpecificationObject(String femObjectPrependNameInitial, int nodeStartIdInitial, boolean nodeIdOffsetInitial, int elementStartIdInitial, boolean elementIdOffsetInitial, int physicalPropertyTableStartIdInitial, boolean physicalPropertyTableIdOffsetInitial)
femObjectPrependNameInitial
- String to prepend to fem object names such as element collector, material and sectionnodeStartIdInitial
- Start id to use for imported nodesnodeIdOffsetInitial
- If true node_start_id will be used as an offset for imported node idselementStartIdInitial
- Start id to use for imported elementselementIdOffsetInitial
- If true element_start_id will be used as an offset for imported element idsphysicalPropertyTableStartIdInitial
- Start id to use for imported physical property tablesphysicalPropertyTableIdOffsetInitial
- If true physical_property_table_start_id will be used as an offset for imported physical property table idsCopyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.