public interface CfdContactPreventionConstraintCollection extends TaggedObjectCollection
CAE.CfdContactPreventionConstraint
in a fem part
BaseFEModel
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
CfdContactPreventionConstraint |
cloneConstraint(CfdContactPreventionConstraint source)
Clones a contact prevention constraint.
|
CfdContactPreventionConstraintBuilder |
createBuilder(TaggedObject recipe)
Creates a local resolution constraint builder
License requirements: nx_adv_fluid_mod ("NX Advanced Fluid Modeling") . |
void |
deleteConstraint(CfdContactPreventionConstraint constraint)
Delete a contact prevention constraint.
|
CfdContactPreventionConstraint |
findObject(String journalIdentifier)
Finds the
CAE.CfdContactPreventionConstraint with the given identifier as recorded in a journal. |
_find_next, iterator
CfdContactPreventionConstraint findObject(String journalIdentifier) throws NXException, RemoteException
CAE.CfdContactPreventionConstraint
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Local Resolution Constraint nameNXException
RemoteException
CfdContactPreventionConstraintBuilder createBuilder(TaggedObject recipe) throws NXException, RemoteException
recipe
- CfdContactPreventionConstraint
to be edited,
if null or FluidDomainRecipe
then create a new oneNXException
RemoteException
void deleteConstraint(CfdContactPreventionConstraint constraint) throws NXException, RemoteException
constraint
- The contact prevention constraint to be deletedNXException
RemoteException
CfdContactPreventionConstraint cloneConstraint(CfdContactPreventionConstraint source) throws NXException, RemoteException
source
- Source contact prevention constraintNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.