public interface BoltCollection extends TaggedObjectCollection
BaseFEModel
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
BoltBuilder |
createBoltBuilder(Bolt bolt)
Creates a builder for Bolt Command
License requirements: nx_masterfem ("Finite Element Modeling") . |
Bolt |
findObject(String journalIdentifier)
Finds the
Bolt with the given identifier as recorded in a journal. |
_find_next, iterator
Bolt findObject(String journalIdentifier) throws NXException, RemoteException
Bolt
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Bolt nameNXException
RemoteException
BoltBuilder createBoltBuilder(Bolt bolt) throws NXException, RemoteException
bolt
- Bolt
to be edited.
if null then create a new oneNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.