Package | Description |
---|---|
nxopen.bodydes |
Provides classes and interfaces for Body Design.
|
Modifier and Type | Field and Description |
---|---|
static OnestepUnformBuilder.Surface |
OnestepUnformBuilder.Surface.INNER
Onestep solver will offset inner surface and enlarge it
|
static OnestepUnformBuilder.Surface |
OnestepUnformBuilder.Surface.MIDDLE
Onestep solver will not offset middle surface
|
static OnestepUnformBuilder.Surface |
OnestepUnformBuilder.Surface.OUTER
Onestep solver will offset outer surface and shrink it
|
Modifier and Type | Method and Description |
---|---|
OnestepUnformBuilder.Surface |
OnestepUnformBuilder.surfaceType()
Returns the surface type used to determine offset direction.
|
static OnestepUnformBuilder.Surface |
OnestepUnformBuilder.Surface.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnestepUnformBuilder.Surface |
OnestepUnformBuilder.Surface.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnestepUnformBuilder.Surface[] |
OnestepUnformBuilder.Surface.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OnestepUnformBuilder.setSurfaceType(OnestepUnformBuilder.Surface surfaceType)
License requirements: nx_onestep_analysis ("NX Onestep Analysis") OR ug_body_design ("Body Design") OR die_engineering ("DIE ENGINEERING") OR aero_sheet_metal ("Aerospace Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.