Package | Description |
---|---|
nxopen.bodydes |
Provides classes and interfaces for Body Design.
|
Modifier and Type | Field and Description |
---|---|
static OnestepUnformBuilder.Object |
OnestepUnformBuilder.Object.FACE
face
|
static OnestepUnformBuilder.Object |
OnestepUnformBuilder.Object.SOLID
solid
|
Modifier and Type | Method and Description |
---|---|
OnestepUnformBuilder.Object |
OnestepUnformBuilder.objectType()
Returns the object type for onestep unform.
|
static OnestepUnformBuilder.Object |
OnestepUnformBuilder.Object.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnestepUnformBuilder.Object |
OnestepUnformBuilder.Object.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnestepUnformBuilder.Object[] |
OnestepUnformBuilder.Object.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OnestepUnformBuilder.setObjectType(OnestepUnformBuilder.Object objectType)
License requirements: nx_onestep_analysis ("NX Onestep Analysis") OR ug_body_design ("Body Design") OR die_engineering ("DIE ENGINEERING") OR aero_sheet_metal ("Aerospace Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.