Package | Description |
---|---|
nxopen.bodydes |
Provides classes and interfaces for Body Design.
|
Modifier and Type | Field and Description |
---|---|
static OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.DisplaySpringbackMode.ALONGX
Onestep display springback mode is along X
|
static OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.DisplaySpringbackMode.ALONGY
Onestep display springback mode is along Y
|
static OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.DisplaySpringbackMode.ALONGZ
Onestep display springback mode is along Z
|
static OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.DisplaySpringbackMode.DISPLACEMENT
Onestep display springback mode is displacement
|
Modifier and Type | Method and Description |
---|---|
OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.solverDisplaySpringbackMode()
Returns the option for springback display.
|
static OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.DisplaySpringbackMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnestepUnformBuilder.DisplaySpringbackMode |
OnestepUnformBuilder.DisplaySpringbackMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnestepUnformBuilder.DisplaySpringbackMode[] |
OnestepUnformBuilder.DisplaySpringbackMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OnestepUnformBuilder.setSolverDisplaySpringbackMode(OnestepUnformBuilder.DisplaySpringbackMode solverDisplaySpringbackMode)
License requirements: nx_onestep_analysis ("NX Onestep Analysis") OR ug_body_design ("Body Design") OR die_engineering ("DIE ENGINEERING") OR aero_sheet_metal ("Aerospace Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.