Package | Description |
---|---|
nxopen.bodydes |
Provides classes and interfaces for Body Design.
|
Modifier and Type | Field and Description |
---|---|
static OnestepUnformBuilder.Constraint |
OnestepUnformBuilder.Constraint.CURVE_ALONG_CURVE
Curve along Curve Constraint, used for complete unform only
|
static OnestepUnformBuilder.Constraint |
OnestepUnformBuilder.Constraint.CURVE_TO_CURVE
Curve to Curve Constraint, used for intermediate unform only
|
static OnestepUnformBuilder.Constraint |
OnestepUnformBuilder.Constraint.POINT_TO_POINT
Point to Point Constraint, used for complete unform only
|
Modifier and Type | Method and Description |
---|---|
OnestepUnformBuilder.Constraint |
OnestepUnformBuilder.constraintType()
Returns the constraint type for intermediate unform or complete unform.
|
static OnestepUnformBuilder.Constraint |
OnestepUnformBuilder.Constraint.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnestepUnformBuilder.Constraint |
OnestepUnformBuilder.Constraint.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnestepUnformBuilder.Constraint[] |
OnestepUnformBuilder.Constraint.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OnestepUnformBuilder.setConstraintType(OnestepUnformBuilder.Constraint constraintType)
License requirements: nx_onestep_analysis ("NX Onestep Analysis") OR ug_body_design ("Body Design") OR die_engineering ("DIE ENGINEERING") OR aero_sheet_metal ("Aerospace Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.