public static interface Tree.StateIconNameCallback
BlockStyler.Node#setState
and the corresponding
state icon of node state is not known. This callback is expected to provide
the icon name for the node state used in the application. This callback is
called only once for any given node state.Modifier and Type | Method and Description |
---|---|
String |
stateIconNameCallback(Tree tree,
Node node,
int state)
Represents the callback which gets called when the node state is set
by
BlockStyler.Node#setState and the corresponding
state icon of node state is not known. |
String stateIconNameCallback(Tree tree, Node node, int state) throws NXException, RemoteException
BlockStyler.Node#setState
and the corresponding
state icon of node state is not known. This callback is expected to provide
the icon name for the node state used in the application. This callback is
called only once for any given node state.
tree
- Tree.node
- Node.state
- Node state for which callback is expected to return state icon name.NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.