Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AttributeSearchTermBuilder
An AttributeSearchTermBuilder is used to create or edit an
AttributeSearchTerm . |
interface |
BoxSearchTermBuilder
A BoxSearchTermBuilder is used to create or edit an
BoxSearchTerm . |
interface |
PlaneSearchTermBuilder
A PlaneSearchTermBuilder is used to create or edit an
PlaneSearchTerm . |
interface |
ProximitySearchTermBuilder
A ProximitySearchTermBuilder is used to create or edit an
Assemblies.BoxSearchTerm . |
Modifier and Type | Method and Description |
---|---|
void |
SubsetRecipe.addSearchTermBuilder(SearchTermBuilder searchTermBuilder)
Add a
SearchTermBuilder to the recipe. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.