Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.ComponentLayerOption.AS_SPECIFIED
Set the specified layer
|
static ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.ComponentLayerOption.MAINTAIN
Maintain the layer of the component being replaced out
|
static ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.ComponentLayerOption.ORIGINAL
Set the layer to replacement part's original layer
|
static ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.ComponentLayerOption.WORK
Set the layer to current work layer
|
Modifier and Type | Method and Description |
---|---|
ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.componentLayerOptionType()
Returns the layer options
License requirements: None. |
static ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.ComponentLayerOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReplaceComponentBuilder.ComponentLayerOption |
ReplaceComponentBuilder.ComponentLayerOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReplaceComponentBuilder.ComponentLayerOption[] |
ReplaceComponentBuilder.ComponentLayerOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ReplaceComponentBuilder.setComponentLayerOptionType(ReplaceComponentBuilder.ComponentLayerOption componentLayerOption)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.